Smart Factory
The Smart Factory is a central concept of Industry 4.0 and represents the next stage in the development of industrial production. It describes a fully networked, data-driven production environment in which machines, systems, and people work together in real time.
Companies in the mechanical engineering and manufacturing industries can produce more efficiently, flexibly, and sustainably with smart production systems. Mitsubishi Electric supports the transition to the smart factory with innovative automation and digitalization solutions.
What is a Smart Factory?
A Smart Factory is a factory that enables autonomous and optimized production through the use of digital technologies such as the Internet of Things (IoT), artificial intelligence (AI), cloud systems, and automation. Systems in the smart factory communicate with each other continuously, exchange data, and adapt dynamically to new requirements. The goal is to achieve maximum transparency and efficiency in manufacturing processes while reducing resource consumption and error rates. Production planning is data-driven and the production environment is flexibly adaptable.
“A Smart Factory is a networked production facility in which machines, sensors, and IT systems work together in a coordinated and automated manner to increase efficiency, quality, and flexibility.”
Importance for the industry
The Smart Factory is defined not only by technology, but also by the intelligent organization of manufacturing processes. For companies, this means faster time-to-market, less waste, lower production costs, and higher product quality. The ability to respond to customer requests and market changes in real time is particularly relevant. Smart manufacturing systems are leading to a profound transformation of traditional production systems into cyber-physical networks that continuously learn and optimize.
Advantages of a Smart Factory
The introduction of a Smart Factory opens up a wide range of opportunities for companies to make their production more efficient, flexible, and future-proof. One of the biggest advantages is the significantly increased transparency: every production step can be tracked and evaluated in real time. This not only makes it easier to monitor processes, but also to continuously improve them. At the same time, digital networking enables a quick response to market and customer requirements. Production processes can be flexibly adapted so that companies can deliver their products faster and in a more customized manner.
The Smart Factory also demonstrates its strengths in terms of efficiency. The use of automation, predictive maintenance, and intelligent self-diagnostics reduces downtime and optimizes the use of resources. This lowers production costs and at the same time increases product quality, as sources of error can be identified and eliminated at an early stage. Overall, the Smart Factory leads to a significant increase in competitiveness because companies can produce faster, more cost-effectively, and with higher quality.
Challenges on the path to the Smart Factory
As attractive as the advantages are, there are a number of hurdles to overcome. The high investment costs for new technologies and infrastructure are particularly significant. Many companies are also faced with the question of how to integrate existing systems into the digital environment. While a completely new factory can be planned relatively easily using the greenfield approach, modernizing existing systems—the so-called brownfield approach—often requires significantly more effort and complex transitional solutions.
In addition, issues such as IT security and data protection play a crucial role. With increasing connectivity, the risk of cyberattacks and data loss also rises, making a well-thought-out security concept indispensable. Added to this is the shortage of skilled workers: qualified personnel are needed to operate and further develop digital processes, but they are not always available in sufficient numbers.
Another obstacle is the lack of uniform technical standards. Open interfaces and common standards are needed to enable machines and systems from different manufacturers to communicate smoothly with each other. Finally, the human factor should not be underestimated: digital transformation is fundamentally changing working methods and structures. Communication, training, and careful change management are essential to ensure that employees actively support these changes.
Smart Factory Solutions from Mitsubishi Electric
Mitsubishi Electric offers a comprehensive portfolio of Smart Factory Solutions covering all levels of automation. These include PLC systems (MELSEC), motion controllers, HMI systems, SCADA, edge and cloud solutions, and AI-based analytics. The particular focus is on modularity, scalability, and integration into existing manufacturing systems. The “e-F@ctory concept” enables end-to-end communication from the factory floor to the cloud.
| Component | Function & Benefits | Typical application |
| MELSEC SPS | Real-time control and safety | Production lines in mechanical |
| GOT HMI | Operation & visualization of machine statuses | Control panels in production cells |
| SCADA-Systeme | Monitoring & analysis of entire production environments | Plant control in large-scale production |
| Edge Computing
(Edgecross) | Local data analysis without cloud dependency | Condition monitoring of machines |
| Predictive Maintenance | Predictive Maintenance based on AI | Minimization of downtime |
With their reliable, proven performance and future-proof expandability the MELSEC series allow a wide range of control applications.
Enhance operator user experience whether in front of the machine or using remote access. Open the window to your machine. Unlock the full power of automation.
Visualize, monitor, and control your enterprise with the industry's best SCADA solution.
Mitsubishi Electric industrial computer MELIPC offers new values for Edge computing, IT system coordination, and device control with its robust features and flexibility utilizing general purpose applications.
Smart Factory examples from practice
Smart Factory concepts are no longer a vision of the future, but are already being successfully implemented in a wide variety of industries today. Practical examples demonstrate the tangible benefits of smart manufacturing—in terms of efficiency, flexibility, and cost savings, for example. The following applications show how companies have been able to achieve measurable improvements through networked production systems, intelligent machines, and digital planning. Intelligent automation can deliver enormous productivity gains, particularly in mechanical engineering, the automotive industry, and electronics manufacturing.
Networked machines with self-diagnostics
In the automotive industry, production machines continuously send data to a central monitoring system. Faults and wear are automatically detected before production comes to a standstill. This significantly reduces downtime and increases plant availability. At the same time, maintenance intervals can be planned much more precisely and customized based on this data. This avoids unnecessary maintenance while ensuring that critical interventions are carried out in a timely manner. In addition, early fault detection helps to ensure production quality, as problems can be corrected immediately. Continuous transparency across the entire machine park also makes it easier to optimally control capacities and improve utilization.
Flexible production cells with automatic changeover
In der Elektronikfertigung erkennen Maschinen neue Produkte automatisch und stellen sich selbstständig auf die erforderlichen Parameter ein. Rüstzeiten entfallen vollständig, was die Effizienz in der Variantenfertigung erheblich steigert. Dadurch können auch Kleinserien oder kundenspezifische Anpassungen wirtschaftlich umgesetzt werden, ohne dass dafür lange Umrüstphasen einkalkuliert werden müssen. Zudem lassen sich Produktionskapazitäten dynamisch verteilen, sodass Engpässe minimiert und Aufträge schneller abgearbeitet werden können. Die höhere Flexibilität ermöglicht es Unternehmen, unmittelbar auf Veränderungen im Markt oder spezifische Kundenanforderungen zu reagieren.
Digitale Zwillinge in der Produktionsplanung
Digital twins are increasingly being used in metalworking to simulate production processes before they actually start. Bottlenecks and potential sources of error are identified at an early stage and can be specifically avoided. This digital simulation not only saves material and time, but also reduces waste, thereby lowering production costs in the long term. An additional advantage is the ability to test new machine configurations virtually. This allows companies to significantly reduce investment risks, as the effects of planned changes become visible in advance. Continuous feedback of real-time data from ongoing production means that the digital models are constantly refined and further optimized. In this way, various scenarios can be played out before any interventions are made in real production.
Smart Factory im Maschinenbau – Chancen und Herausforderungen
Smart Factory technologies open up a wide range of opportunities in mechanical engineering. Predictive maintenance, adaptive manufacturing, real-time monitoring, and automated quality assurance are among the key innovations. They shorten manufacturing processes, reduce production costs, and simultaneously increase the quality of end products. The scalability of these technologies is particularly attractive: even medium-sized companies can gradually transition to the Smart Factory and expand digitalization as needed.
Nevertheless, challenges remain, particularly in the area of interoperability. Open interfaces and common standards are necessary to ensure that systems from different manufacturers work together seamlessly. Investing in employee training is equally important. Only when the necessary expertise is available can the potential of smart machines be fully exploited and the transformation successfully implemented.
Sustainability in the Smart Factory
Smart Factories play a key role in making production processes more environmentally friendly. Energy consumption is significantly reduced through targeted control of processes and demand-based utilization of machines. At the same time, precision manufacturing ensures that less material is wasted and scrap is avoided.
Predictive Maintenance also plays an important role: it extends the service life of machines, prevents unplanned downtime, and thus reduces the need for spare parts. Companies that digitize their production not only achieve efficiency gains, but also make a measurable contribution to greater sustainability and the achievement of their ESG goals.
FAQ – Frequently asked questions about IoT
What is a Smart Factory in simple terms?
A smart factory is an intelligent, digitally networked factory in which machines, systems and people work together, organise themselves and adapt processes automatically.
What are the advantages of a smart factory for companies?
It increases efficiency and product quality, reduces downtimes through predictive maintenance and enables fast reactions to market changes.
What do you need to set up a smart factory?
Networkable machines with sensors, control systems such as PLCs and HMIs, data platforms for analysis and interfaces for IT and OT integration are required.
Is the Smart Factory also relevant for smaller companies?
Yes, modular and scalable systems allow a gradual entry, also through smart retrofit solutions for individual areas.
What distinguishes Mitsubishi Electric from other suppliers?
Mitsubishi Electric offers complete solutions from a single source, open platforms, high integration capability and practical advice based on many years of industry experience.
We are pleased to advise you personally!