News Releases
FOR IMMEDIATE RELEASE No. 3329
UPDATED, February 20, 2020 - Although Mitsubishi Electric was, at the time of the original press release, planning to participate and exhibit the new product at embedded world 2020 in Nuremberg, Germany from February 25 to 27, decision has been made not to.
TOKYO, January 23, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of a 7.0-inch WVGA TFT-LCD module equipped with a built-in short-range NFC1 antenna and a projected capacitive touch panel. The new module is designed for use in a wide range of applications such as access control system terminals. Sample sales will begin on March 31, 2020 via Mitsubishi Electric offices worldwide.
Mitsubishi Electric Color TFT-LCD module with NFC antenna projected capacitive touch panel Model AN070MC11ADA11
With their built-in NFC antennas, the new modules will save space, offer improved ease of use and boost the deployment of NFC-enabled services and devices.
The new products will be exhibited at embedded world 2020 in Nuremberg, Germany from February 25 to 27.
Product | Model | Display Size | Resolution | Sample Shipments |
---|---|---|---|---|
TFT-LCD Modules with NFC antenna and Projected Capacitive Touch Panels | AN070MC11ADA11 | 7.0-inch | WVGA | March 31, 2020 |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.