Industry trends in servo drives: Creating new quality with Melservo J5 Part 2
23.04.202510 min read
The second part of the article on industry trends in servo drives addresses further challenges such as limited manufacturer warranties, rising energy costs, and the growing use of predictive maintenance to optimize maintenance.
The future of servo systems: an overview of challenges and trends (Part 2/2)
The challenge of limited warranty and support periods offered by servo system manufacturers
The duration of manufacturer warranties and support is not only relevant for end customers, but also affects system integrators and machine builders. There is consensus that automation technology providers should support their products for as long as possible. On average, most manufacturers offer support and replacement parts for discontinued product lines for around ten years after they are withdrawn from the market¹. But what happens after that?
Users are often left with no choice but to replace all drive components at great expense or search for used replacement parts – because only a few manufacturers guarantee consistent backward compatibility between old and new series².
Mitsubishi Electric has been committed to sustainability through long-term backward compatibility for many years. One example: The MR-J5 series is partially compatible with the MR-J2S series, which is over 25 years old, via its mounting interface. It is also fully compatible with the MR-J4 series, enabling a smooth transition and simplifying upgrades.
What does this backward compatibility mean in concrete terms?
Same connection dimensions for motors and servo drives
Operation of MR-J4 motors with the MR-J5 series
Special versions of the drives (MR-J5-B) with SSCNETIII/H interface for existing networks
Shared use of older and newer servo drive series within an application in compatibility mode
Software tools for easy parameter transfer between generations
Mitsubishi Electric thus ensures backward compatibility on multiple levels – both in hardware and software.
Of course, the option to migrate is only part of the picture. That's why Mitsubishi Electric devices are designed to remain reliable in operation for at least ten years – even components with high wear potential such as smoothing capacitors. Mitsubishi Electric also ensures that spare parts are available for up to 20 years after the end of series production.
Combined with backward compatibility, this offers decisive advantages:
Lower operating costs thanks to durable and robust components
Minimized downtime thanks to long-term spare parts availability
Greater confidence in a manufacturer that focuses on sustainability and quality
___________________________________________
[1] Average data from the ten leading servo drive manufacturers on the European market.
[2] Only one in ten companies surveyed guarantees complete backward compatibility.
Rising energy prices and legal requirements – new demands on modern servo systems
Energy crisis, emissions trading, legislation: electricity price trends in Germany
Electricity prices in Germany have risen significantly in recent years. Energy-intensive industries are particularly feeling the financial impact of this development.
A key factor is the European Emissions Trading System (EU ETS), which requires companies to purchase emissions allowances. Rising allowance prices are driving energy costs even higher. In addition, the war in Ukraine has led to an energy crisis that has caused electricity and gas prices to skyrocket.
The German government is attempting to provide short-term relief with its 2024/2025 electricity price package, but forecasts indicate that prices will continue to rise in the long term. The high volatility of electricity prices is particularly problematic, forcing many companies to purchase electricity on the spot market.
In addition, strict legal requirements apply to energy efficiency. Regulations such as the Energy Efficiency Act (EnEfG) or the EU Directive 2010/75/EU on industrial emissions (IED) require a reduction in energy consumption, which often means high investments.
According to current electricity price trends, the price for industrial companies in 2024 was around 15.16 ct/kWh for procurement, grid fees, and distribution, while levies stood at 1.43 ct/kWh. In 2022, the total electricity price was still 38.62 ct/kWh. These sharp price fluctuations illustrate the uncertainty of the development.
The price development of electricity and emission allowances shows clear parallels, indicating that prices will continue to rise even after the geopolitical situation stabilizes. EU climate policy, in particular the “Fit for 55” program, suggests that no fundamental relief is to be expected. Companies therefore remain under pressure to optimize their energy efficiency and develop new strategies to reduce costs.
The right drive technology to combat rising energy costs
Although it is difficult to counteract rising prices and energy policy, electricity consumption can be reduced by using energy-efficient devices. One example of such a system is the MR-J5D DC bus system.
In this system, the servo drives operate within a common DC bus and benefit from the phenomenon of energy recovery. This means that the mechanical energy generated when the drive brakes (for example, when a vertical axis moves down) is fed back into the servo system. This recovered energy is then distributed to other drives that are active in the drive cycle. In contrast to standard solutions, where the energy generated during regenerative braking is dissipated as heat to the brake resistors, the energy is put to good use here.
Depending on the application, the MR-J5D series servo amplifiers can reduce the power required to operate the servo drive by up to 70%3. In combination with the highly efficient servo motors of the HK series (with an average efficiency of 90% in the power range from 0.1 to 2 kW), the power consumption and operating costs of the drive system can be significantly reduced.
The adjacent illustration shows the structure of the MR-J5D drive series.
___________________________________________
[3] Source: A. Buryło: “Assessment of the influence of regenerative systems on the energy efficiency of servo drives,” Krakow, 2023, Krakow University of Technology
Intelligent servo drives: How AI is advancing maintenance to predictive maintenance
For at least a year now, we have been intensively engaged with the topic of artificial intelligence in all its facets. It is now almost impossible to find someone who has never heard of ChatGPT or other AI-based tools that support us in our everyday tasks, whether at work or in our private lives. But how does artificial intelligence find its way into industrial automation? Many would probably point to complex, distributed systems based on powerful servers and cloud computing. But that is not necessarily the case. Artificial intelligence can also be used in smaller applications and integrated into standard devices such as industrial robots, frequency converters, or servo drives.
An outstanding example of the use of state-of-the-art AI technology is Maisart, Mitsubishi Electric's artificial intelligence, which is used in many automation devices. A particularly clear example of its application is the predictive maintenance function – a machine diagnosis function integrated into the servo amplifiers of the MELSERVO J5 series. This function enables a predictive approach to be applied not only to the drive components themselves, but also to the associated mechanical systems such as ball screws, belt and gear drives, and mechanical gearboxes.
The machine diagnostics function allows the servo drive to be used not only as an actuator in the application, but also as an advanced sensor. The servo drive can check the current status and predict the first signs of mechanical component failure based on estimated friction and vibration values for ball screw drives or values for belt tension changes in belt drives.
By using these functions, downtime in production facilities can be significantly reduced at minimal maintenance costs, as every drive in the MR-J5 series is equipped with them as standard. Artificial intelligence (AI) is often associated with complex algorithms whose implementation requires specialist knowledge. However, Maisart, the AI technology in the servo drives, uses machine learning to solve precisely this problem. Setting up and activating the AI-supported maintenance functions is extremely simple and takes only a few minutes. The entire process is limited to configuring a few parameters directly in the servo amplifier.
Integrated machine diagnostics represent an important step toward predictive maintenance – a core element of Industry 4.0. Any manufacturing company that wants to remain competitive in the long term should embrace this development. The use of AI-supported predictive maintenance not only increases customer confidence in the machines, but also significantly improves ease of maintenance. Thanks to intelligent machine diagnostics, necessary maintenance measures and component replacements can be identified and planned at an early stage – without the risk of unexpected downtime and associated costs.
___________________________________________
[6] The global market for Industry 4.0 is expected to reach a volume of US$165.5 billion by 2026, compared to US$73.9 billion in 2022, representing an annual growth rate of 20.6% (growth between 2021 and 2022 was 39.12%). Source: “Industry 4.0 Market Size, Share & Industry Growth Analysis Report by Technology (Industrial Robots, Blockchain, Industrial Sensors, Industrial 3D Printing, Machine Vision, HMI, AI in Manufacturing, Digital Twin, AGV's, Machine Condition Monitoring) and Geography - Global Growth Driver and Industry Forecast to 2026,” Market&Markets
Summary
We hope this article has given you a concise insight into the latest developments in the mechanical engineering industry. This industry is constantly changing, with increasing demands on energy efficiency, maintenance strategies, and future-proofing. Mitsubishi Electric is growing with these demands, and the MELSERVO J5 series has been developed precisely for this purpose: for energy-efficient operation, AI-supported predictive maintenance, and maximum backward compatibility.
Of course, we cannot cover all functions and parameters in one article. Please visit our product page to learn more about the MR-J5 series and other servo drives in our portfolio.
Download the flyer here and learn more about the MELSERVO MR-J5 servo motion system. Discover advanced servo technology with AI-based maintenance, high-performance amplifiers, and seamless network integration for maximum precision and efficiency.
Download the flyer here and learn more about the MELSERVO MR-J5 servo motion system with EtherCAT. Discover Safety over EtherCAT (FSoE), powerful servo drives, and precise servo motors for maximum efficiency and flexibility in your production.
Download the flyer here and learn more about the advantages of Servo Open Network and the flexible application of the MELSERVO MR-J4 servo series. Find out in detail about the seamless integration of open network connections and how you can optimize your production processes.
Servo drives in the changing world of industry – read more now
In the first part of our blog series, we take a look at the most important trends shaping the use of modern servo drives. Find out how Mitsubishi Electric's MR-J5 series provides