News Releases

Mitsubishi Electric Develops Extra-thin Antenna Technology for Inflight ConnectivityNew antenna and RF-IC will enable future high-speed internet access even in small aircraft

FOR IMMEDIATE RELEASE No. 3334

TOKYO, February 6, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that in collaboration with Japan's National Institute of Information and Communications Technology (NICT) it has developed technology for an extra-thin Ka-band (27 to 40 GHz) active electronically steered array antenna (AESA) featuring the world's thinnest* profile, less than three centimeters, to deliver high-speed inflight connectivity services via satellites at data rates beyond 100 Mbps. The company also announced that it has developed the antenna elements and, in collaboration with Tohoku University and Tohoku MicroTec Co., developed a radio-frequency integrated circuit (RF-IC) for an envisioned millimeter-wave V-band (40 to 75 GHz) AESA that will be capable of delivering inflight connectivity at even faster speeds.

  1. *According to internal research as of February 6, 2020.

Mitsubishi Electric's new Ka-band AESA is thin and small enough to be installed in any aircraft, regardless of its size, and it can operate even at high latitudes, which will allow passengers to enjoy on-demand streaming and other high-speed internet services on flights worldwide. Following further testing and demonstrations, the company plans to commercialize its Ka-band AESA after 2023 and a V-band AESA after 2027.

Rendition of Mitsubishi Electric's AESA

Features

  1. 1)Extra-thin AESA for high-speed satellite communication even at high latitudes in diverse aircraft
    • Conventionally bulky antennas for satellite communication are not easily installed in small and midsize aircraft because of the space required for the antennas and the devices that mechanically drive them. Mitsubishi Electric has now solved this problem by incorporating antenna elements newly developed by NICT and Mitsubishi Electric's RF combiner/divider and RF-ICs into a single circuit board, and then combining them in a Ka-band AESA featuring the world's thinnest profile of less than three centimeters.
    • Mitsubishi Electric also has newly developed a proprietary millimeter-wave antenna with a hollow cavity inside a printed circuit board, which improves the antenna's circular-polarization quality and electric-power efficiency. The proprietary antenna ensures high performance even when beam steering at an elevation angle of as low as 20 degrees, thereby enabling operation in the high latitudes.

    Structure of Mitsubishi Electric's millimeter-wave antenna

  2. 2)Ka- and V-band RF-ICs for inflight connectivity via next-generation high-throughput satellites
    • High-power and low-noise amplifiers for transmission/reception circuitry are needed to miniaturize satellite-communication antennas as well as improve their performance. Mitsubishi Electric's new Ka-band RF-IC incorporates a high-power amplifier boasting an unprecedented power-added efficiency rating of 29.1% (when converting DC input power to RF output signals), 1.8 times that of an existing RF-IC made by Mitsubishi Electric. Also, the RF-IC's low-noise amplifier achieves an unprecedentedly low noise figure of just 1.8dB, about 20 percent lower than that of a conventional model.
    • For Mitsubishi Electric's next-generation V-band AESA, RF-ICs are being miniaturized for arraying at narrower intervals than in the case of the Ka-band AESA. Mitsubishi Electric, in collaboration with Tohoku University and Tohoku MicroTec Co., Ltd., has developed the world's first three-dimensionally integrated millimeter-wave RF-IC, which it stacks in pairs using a through-silicon vias.

    Mitsubishi Electric's three-dimensionally integrated millimeter-wave RF-IC


Note

Note that the press releases are accurate at the time of publication but may be subject to change without notice.


Inquiry

Media contact

Customer Inquiries